Source Control > Add to Source Control command
Choose this command to initiate a check in operation.
Note that this menu item displays only if all of the following conditions exist:
- an open project exists
- no association exists between the open project and any file under source control.
Provide Feedback