Industrial engineers can more efficiently design and configure stand-alone machines using the latest release of Connected Components Workbench software from Rockwell Automation.
With several new and enhanced features, the software improves download and build performance to create more efficient, user-friendly design processes.
Highlights of what’s new in version 13 of Connected Components Workbench software include:
- A new Global and Local variable data grid that delivers capabilities to help engineers develop projects faster. For example, a quick declaration feature allows users to create multiple variables with the same prefix, suffix and data type in one click. An intuitive filter bar allows users to find tags quickly.
- An enhanced Run Mode Change (RMC) capability that enables users to make edits without downloading project source code. This can speed up online edits and create smoother, more seamless design experiences.
- A new Controller Organizer view that gives engineers the option to switch to a Logix Theme programming experience. This allows them to work in a more familiar environment and use copy-and-paste ladder logic from the Studio 5000 Logix Designer application.
- An enhanced Global Connection capability on existing system tags in the PanelView 800 DesignStation that gives users greater flexibility to configure remote system connections.
The Connected Components Workbench software helps simplify the development of stand-alone machines that are built with the Rockwell Automation Micro Control system. Engineers can configure, program and visualize the major control components of their stand-alone machines in a single software environment. They can also use tools like the Micro800 Simulator to validate their application code without the need for hardware.
Allen-Bradley, Connected Components Workbench, expanding human possibility, FactoryTalk, Micro800, PanelView, Rockwell Automation, Studio 5000, and Studio 5000 Logix Designer are trademarks of Rockwell Automation Inc. Trademarks not belonging to Rockwell Automation are property of their respective companies.