Smart Object properties

These are the Smart Object properties.
Element
Description
Desc
Description. Information that describes the Smart Object.
Version
Version information for the Smart Object. String formatted as major.minor.build. Each revision number can be 0 to 999. If there is no period, the number is treated as a major revision only.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.