Open a project

  1. Close any open project.
  2. To open a project, either:
    • On the
      Welcome
      page, select
      Open project
      .
    • On the
      Welcome
      page, select a project from the
      Recent projects
      list.
    • From the menu bar, select
      File > Open project
      .
  3. In
    Open project
    , in
    Open from
    , select the location of the project:
    • Local
      . Open a project from your local workspace.
    • Remote
      . Open a project from the shared repository.
  4. Select the project to open.
  5. Select
    Open
    .
    TIP: You cannot open a project from the shared repository when it already exists in your local workspace. Open the local project.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.