Search for cross-references

Use the cross-reference feature to search for all tag references. A cross-reference tag returns all routine references, including the instruction type and if the reference is destructive.
To search for cross-references
  1. Open the tag from either the Ladder Diagram or Tag Editor.
    • From the Ladder Diagram, right-click the tag and select
      Find all references
      .
    • From the Tag Editor, right-click the first cell of the tag row and select
      Find all references
    A new tab opens that contains a list of the routines in which the tag is referenced, grouped by program.
    TIP: If no references exist for the tag, the message
    No references were found
    shows in the cross-reference tab.
  2. If it is not already expanded, select the caret to expand the program to view the routines that reference the tag.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.