Import Sections
Use the
Import Sections
option to add sections to existing lineups. Prerequisites
- Purchase and download the dataset folder.
- Unzip the dataset folder to your local drive.
- AFactoryTalk Design Studioproject with lineups.
To add sections to an existing lineup:
- From the IntelliCENTER MCC lineup explorer tree, right-click and selectImport Sections. TheImport Sectionsdialog box opens.
- To add new sections, selectBrowseunderDocumentationto locate the Sections documentation. The import tool reads the dataset and shows a list of available lineups.
- To replace a door or existing unit, selectBrowseunderDocumentationto locate the replacement Unit documentation.
- Select one or more lineup and selectImport.
Provide Feedback