Import device configuration

Import a device configuration to restore a device to a previous configuration. The configuration contains either one or two configuration files.
  1. On the explorer bar, select Devices Icon
    Devices
    .
  2. In
    Devices
    , right-click a device, and then select
    Properties
    .
  3. In
    Properties
    , select
    Save/Restore
    , then select
    Import
    .
  4. In
    Import
    , complete the following steps:
    1. In the
      Config file
      view, select
      Browse
      to navigate to and import the
      config.text
      or
      startup-config.cfg
      file.
    2. Select
      Open
      , then select
      Next
      .
    3. (optional) If the device also requires a Vlan file, in the
      Vlan file
      view, select
      Browse
      to navigate to and import the
      vlan.dat
      file.
    4. (optional) Select
      Open
      , then select
      Import
      .
  5. Select
    OK
    .
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.