- FactoryTalk Design Studio Help
- Programs, tasks, and routines
- Add-On Instructions
- FactoryTalk Design Studio Code editor
- Instructions
- Instruction set
Updated instruction mnemonics
These instruction mnemonics have been updated to conform to IEC 61131-3 and PLCopen standards.
Instruction | Mnemonic in versions 1.05 and earlier | Mnemonic in versions 1.06 and later |
---|---|---|
Arc Cosine | ACS | |
Arc Sine | ASN | |
Arc Tangent | ATN | |
Convert to BCD | TOD | |
Convert to Integer | FRD | |
Equal To | EQU | |
Greater Than | GRT | |
Greater Than or Equal To | GEQ | |
Less Than or Equal To | LEQ | |
Less Than | LES | |
Limit | LIM | |
Move | MOV | |
Not Equal To | NEQ | |
Square Root | SQR | |
Truncate | TRN | |
X to the Power of Y | XPY |
Provide Feedback