Edit Organization

Edit Organization

The owner or administrator of an organization can edit their organizations by selecting Edit Organization in the FactoryTalk Hub menu.
From the Edit Organization screen you can:
  • Change the name, description, and location of the organization, as well as add an organization logo if so desired.
    NOTE: Images used for organization logos must be smaller than 125 kB.
  • If your organization has a private email domain, you can make the organization publicly visible to other users with the same email domain by selecting the Organization Access checkbox. Leaving the box unchecked means only people who receive an invitation or Join request link you have shared can see and join your organization.
  • Create and copy new Invite Links to let people request access to the organization. When you reset a link from an organization's edit organization page, all previous links to the page become invalid.
  • Select which applications in FactoryTalk Hub are visible to the organization. Check the boxes next to all available applications that you want to be visible to your organization.
  • You can archive organizations that are no longer in use, or that you created by mistake. See Archive Organization
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.