Develop a gauge with a localized engineering unit
Create a linear gauge that displays the current temperature in a format adjusted to the logged in user.
NOTE:
Download a sample project:
ExampleApplication-LocalizedEngineeringUnitGauge.zipPrerequisites
- To develop the project
- Arrange the interface elements.
- Save the project.
In
FactoryTalk Optix Studio
, select to run the project using the client emulator to test your project. To run the project on a remote client, see Add a client device.Provide Feedback