Specify the visibility of a graphic object

Specify the visibility of a graphic object

Determine whether a graphic object is visible in the window at runtime.
  1. In the window or
    Project view
    , select the container or graphic object.
  2. In
    Properties
    , in
    Visible
    , select either:
    • True
      . The graphic object appears in the window at runtime.
    • False
      . The graphic object does not appear in the window at runtime.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.