- Getting started
- Using the software
- OPC UA
- Graphic and layout objects
- Developing solutions
- Developing projects with C#
- Application examples
- UI tutorial
- NetLogic tutorial
- Object and variable references
View alarms in remote local time zone
View alarms in the local time zone to view alarm events remotely.
- SelectTemplate Libraries.
- InTemplate Libraries, drag theAlarm gridorAlarm history gridobject fromWidgetsinto a node in theUIfolder.
- InTemplate Libraries, selectClose.
- InProject view, select the alarm object.
- InProperties, expandTimestamp.
- InText, reset the current value and then selectChange Dynamic Link.
- At the bottom of the window, selectAdvanced...
- In the Advanced Dynamic Link editor, selectInsertand then selectExpression evaluator.
- InExpression, type{0} + {1}and then pressEnter.
- In the{0} DynamicLinkpane, selectChange Dynamic Linkand then selectAlias >{Item} […] > AlarmCondition > Time.
- In{1} DynamicLink, selectChange Dynamic Linkand then selectAlias >{Session} >Session >Time Zone Offset.
- ClickSelect.
Provide Feedback