Add an OPC UA client object

Add an OPC UA client object

Configure an OPC UA (OPC Unified Architecture) client by adding an OPC UA client object to the project and configuring its properties.
  1. In
    Project view
    , right-click
    OPC-UA
    and select
    New
    OPC UA client
    .
  2. In
    Properties
    , set the OPC UA client object properties.
    For more information on the properties, see Object and variable references.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal