Configure a video
Insert a video file container to your project, and place a video file in it. Use video files local to the project or remote videos.
- InProject view, inUI, right-click a container and then select .
- InPath, either:
- SelectBrowseand select the local video to display.TIP:To find items, start typing the item name to find inSelect file.If the file does not appear inSelect file, selectand inImport file(s)Import file(s), select the file to import and then chooseSelect.
- Enter the address of the remote video file to display.
- (optional) Set the auto play options.
- Auto play. Video will be played automatically. Disabled by default.
- Muted. Video will play without sound. Disabled by default.
- Loops. Specifies the number of times video will play. The default is1.
- (optional)Muted.
- (optional) Set theAppearanceandSize and layoutproperties.
video
Provide Feedback