Add a selective divergence (step)
- On theEquipment SequenceElement toolbar, selectAdd Selective Divergence.
- Connect the divergence to a preceding step.
- Add execution paths to the divergence:
- Add and connect a transition to the divergence to create a separate execution path.
- Repeat to create additional execution paths as needed.
- Add and connect additional steps and transitions to each execution path as needed.
- Verify each execution path ends with a transition.
Provide Feedback