One Shot Rising with Input (OSRI)

One Shot Rising with Input (OSRI)

This information applies to the
CompactLogix
5370,
ControlLogix
5570,
Compact GuardLogix
5370,
GuardLogix
5570,
Compact GuardLogix
5380,
CompactLogix
5380,
CompactLogix
5480,
ControlLogix
5580, and
GuardLogix
5580 controllers.
The One Shot Rising with Input (OSRI) instruction sets the output bit for one execution cycle when the input bit toggles from cleared to set.
Available Languages
Ladder Diagram
This instruction is not available in ladder diagram.
Function Block
Structured Text
OSRI(OSRI_tag);
Operands
Structured Text
Operand
Type
Format
Description
OSRI tag
FBD_ONESHOT
Structure
OSRI structure
Function Block
Operand
Type
Format
Description
OSRI tag
FBD_ONESHOT
Structure
OSRI structure
FBD_ONESHOT Structure
Input Parameter
Data Type
Description
EnableIn
BOOL
If cleared, the instruction does not execute and outputs are not updated. If set, the instruction executes.
Default is set.
InputBit
BOOL
Input bit.
Default is cleared.
Output Parameter
Data Type
Description
EnableOut
BOOL
Indicates if instruction is enabled.
OutputBit
BOOL
Output bit
Description
If InputBit is true, and it was false the last time the instruction was scanned then OutputBit will be set, otherwise OutputBit will be cleared.
Affects Math Status Flags
No
Major/Minor Faults
None specific to this instruction. See Common Attributes
for operand-related faults.
Execution
Function Block
Condition/State
Action Taken
Prescan
EnableIn and EnableOut bits are cleared to false.
Tag.Enable-in is false
EnableIn and EnableOut bits are cleared to false.
Tag.Enable-in is true
EnableIn and EnableOut bits are set to true.
The instruction executes.
Instruction first run
N/A
Instruction first scan
Previous InputBit history is set to require a False to True transition of InputBit.
Postscan
EnableIn and EnableOut bits are cleared to false.
Structured Text
Condition/State
Action Taken
Prescan
See Prescan in the Function Block table.
Normal execution
See Tag.EnableIn is true in the Function Block table.
Postscan
See Postscan in the Function Block table
Examples
Function Block
When limit_switch1 goes from cleared to set, the OSRI instruction sets OutputBit for one scan.
Structured Text
OSRI_01.InputBit := limit_switch1;
OSRI(OSRI_01);
State := OSRI_O1.OutputBit;
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal