Convert AC Line Source Config Attrib

Convert AC Line Source Config Attrib

These are the converter AC Line source configuration attributes associated with the AC Line input to a Converter.
AC Line Source Select
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - G
Set/SSV
USINT
0
-
-
Enumeration:
0 = AC Line A
1 = AC Line B (Alternate)
2-255 = Reserved
The AC Line Source Select attribute determines which AC Line source is active for the converter and applies the configured impedance and power rating of that source to the converter's control structure.
AC Line Source Impedance
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - G
Set/SSV
REAL
5
0
100
% Rated Impedance
The AC Line Source Impedance attribute determines the impedance of the AC line source as a percent of the transformer or generator impedance rating.
AC Line Source Power
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - G
Set/SSV
REAL
2500
10*Converter Rated Power
0
Infinity symbol
kVA
The AC Line Source Power attribute sets the power rating of the transformer or generator feeding power to the converter as a percentage of the converter's power rating.
AC Line Source Impedance - Alternate
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - G
Set/SSV
REAL
5
0
100
% Rated Impedance
The AC Line Source Impedance - Alternate attribute determines the impedance of the alternate AC line source as a percent of the transformer or generator impedance rating.
AC Line Source Power - Alternate
Usage
Access
T
Data Type
Default
Min
Max
Semantics of Values
Optional - G
Set/SSV
REAL
100
10*Converter Rated Power
0
Infinity symbol
kVA
The AC Line Source Power - Alternate attribute selects the power rating of the alternate transformer or generator feeding power to the converter as a percentage of the converter's power rating.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.