Process Command Source (PCMDSRC)

Process Command Source (PCMDSRC)

This information applies to the CompactLogix 5380P and ControlLogix 5580P controllers.
The Process Command Source (PCMDSRC) instruction selects the command source for a device.
The instruction includes these command sources:
  • Hand
  • Out-of-Service
  • Maintenance
  • Override
  • External
  • Program locked
  • Program
  • Operator locked
  • Operator
Available Languages
Ladder Diagram
PCMDSRC_ladder
Function Block Diagram
PCMDSRC_FBD
Structured Text
PCMDSRC (PCMDSRC tag);
Operands
IMPORTANT:
Unexpected operation may occur if:
  • Output tag operands are overwritten.
  • Members of a structure operand are overwritten.
  • Except when specified, structure operands are shared by multiple instructions.
There are data conversion rules for mixing numeric data types within an instruction. See Data conversions.
Configuration Operands
Operand
Type
Format
Description
PlantPAx Control
P_COMMAND_SOURCE
tag
Data structure required for proper operation of the instruction.
P_COMMAND_SOURCE Structure
Input Members
Data Type
Description
EnableIn
BOOL
Enable input.
Ladder Diagram:
Corresponds to the rung condition.
Default is true.
Inp_OwnerCmd
DINT
Owner device command:
0 = None,
Inp_OwnerCmd.10 = Operator Lock,
Inp_OwnerCmd.11 = Operator Unlock,
Inp_OwnerCmd.12 = Program Lock,
Inp_OwnerCmd.13 = Program Unlock,
Inp_OwnerCmd.14 = Acquire Maintenance,
Inp_OwnerCmd.15 = Release Maintenance,
Inp_OwnerCmd.16 = Acquire External,
Inp_OwnerCmd.17 = Release External,
Inp_OwnerCmd.29 = Echo.
Default is 0.
Inp_InitializeReq
BOOL
1 = Request to initialize the instruction. The instruction is normally initialized in instruction first run. Use this request when re-initialization is needed. The instruction clears this operand automatically.
Default is true.
Inp_Hand
BOOL
1 = Acquire Hand (typically permanently set to local),
0 = Release Hand.
Default is false.
Inp_Ovrd
BOOL
1 = Acquire Override (higher priority program logic),
0 = Release Override.
Default is false.
Inp_ExtInh
BOOL
1 = Inhibit External acquisition,
0 = Allow External acquisition.
Default is true.
Cfg_HasOper
BOOL
1 = Operator (unlocked) exists, can be selected.
Default is true.
Cfg_HasOperLocked
BOOL
1 = Operator Locked exists, can be selected.
Default is true.
Cfg_HasProg
BOOL
1 = Program (unlocked) exists, can be selected.
Default is true.
Cfg_HasProgLocked
BOOL
1 = Program Locked exists, can be selected.
Default is true.
Cfg_HasExt
BOOL
1 = External exists, can be selected.
Default is false.
Cfg_HasMaint
BOOL
1 = Maintenance exists, can be selected.
Default is true.
Cfg_HasMaintOoS
BOOL
1 = Maintenance Out of Service exists, can be selected.
Default is true.
Cfg_OvrdOverLock
BOOL
1 = Override supersedes Program/Operator Lock,
0 = Do not override Lock.
Default is true.
Cfg_ExtOverLock
BOOL
1 = External supersedes Program/Operator Lock,
0 = Do not override Lock.
Default is false.
Cfg_ProgPwrUp
BOOL
1 = Power up to Program,
0 = Power up to Operator.
Default is false.
Cfg_ProgNormal
BOOL
Normal Source:
1 = Program if no requests,
0 = Operator if no requests.
Default is false.
Cfg_PCmdPriority
BOOL
Command priority.
1 = Program commands win,
0 = Operator commands win.
Default is false.
Cfg_PCmdProgAsLevel
BOOL
1 = PCmd_Prog used as a Level.
Default is false.
Cfg_PCmdLockAsLevel
BOOL
1 = PCmd_Lock used as a Level (1=Lock, 0=Unlock).
Default is false.
Cfg_ExtAcqAsLevel
BOOL
1 = XCmd_Acq used as Level (1 = Acquire, 0 = Release).
Default is false.
PCmd_Oper
BOOL
Program command to select Operator (Program to Operator). The instruction clears this operand automatically.
Default is false.
PCmd_Prog
BOOL
Program command to select Program (Operator to Program). The instruction clears this operand automatically.
Default is false.
PCmd_Lock
BOOL
Program command to lock Program (disallow Operator). The instruction clears this parameter automatically if Cfg_PCmdLockAsLevel = 0.
Default is false.
PCmd_Unlock
BOOL
Program command to unlock Program (allow Operator to acquire). The instruction clears this operand automatically.
Default is false.
PCmd_Normal
BOOL
Program command to select Normal (Operator or Program). The instruction clears this operand automatically.
Default is false.
MCmd_OoS
BOOL
Maintenance command to select Out of Service. The instruction clears this operand automatically.
Default is false.
MCmd_IS
BOOL
Maintenance command to select In Service. The instruction clears this operand automatically.
Default is false.
MCmd_Acq
BOOL
Maintenance command to acquire ownership (Operator/Program/External/Override to Maintenance). The instruction clears this operand automatically.
Default is false.
MCmd_Rel
BOOL
Maintenance command to release ownership (Maintenance to Operator/Program/External/Override). The instruction clears this operand automatically.
Default is false.
XCmd_Acq
BOOL
External command to acquire ownership (Operator/Program/Override/Maintenance to External). The instruction clears this operand automatically if Cfg_ExtAcqAsLevel = 0.
Default is false.
XCmd_Rel
BOOL
External command to release ownership if Cfg_ExtAcqAsLevel = 0 (External to Operator/Program/Override/Maintenance). The instruction clears this operand automatically.
Default is false.
OCmd_Oper
BOOL
Operator command to select Operator (Program to Operator). The instruction clears this operand automatically.
Default is false.
OCmd_Prog
BOOL
Operator command to select Program (Operator to Program). The instruction clears this operand automatically.
Default is false.
OCmd_Lock
BOOL
Operator command to lock Operator (disallow Program). The instruction clears this operand automatically.
Default is false.
OCmd_Unlock
BOOL
Operator command to unlock / release (allow Program to acquire) ownership. The instruction clears this operand automatically.
Default is false.
OCmd_Normal
BOOL
Operator command to select Normal (Operator or Program). The instruction clears this operand automatically.
Default is false.
Output Members
Data Type
Description
EnableOut
BOOL
Enable output. This output state always reflects EnableIn input state.
Sts_Initialized
BOOL
1 = Instruction is initialized. Use Inp_InitializeReq to reinitialize.
Sts_eSrc
INT
The current command source is shown with status bits:
Sts_eSrc.0: Lock,
Sts_eSrc.1: Normal,
Sts_eSrc.2: Hand,
Sts_eSrc.3: Maintenance,
Sts_eSrc.4: Override,
Sts_eSrc.5: Program,
Sts_eSrc.6: Operator,
Sts_eSrc.7: Out of Service,
Sts_eSrc.8: External.
Sts_bSrc
INT
Active selection bitmap (for HMI totem pole with command source request selection)
Sts_bSrc.0: Hand,
Sts_bSrc.1: Programmed Out of Service (rung false),
Sts_bSrc.2: Maintenance Out of Service,
Sts_bSrc.3: Maintenance,
Sts_bSrc.4: Override,
Sts_bSrc.5: External,
Sts_bSrc.6: Program locked,
Sts_bSrc.7: Program,
Sts_bSrc.8: Operator locked,
Sts_bSrc.9: Operator.
Sts_Hand
BOOL
1 = Hand is selected (supersedes OoS, Maintenance, Override, External, Program, Operator).
Sts_OoS
BOOL
1 = Out of Service is selected (supersedes Maintenance, Override, External, Program, Operator).
Sts_Maint
BOOL
1 = Maintenance is selected (supersedes Override, External, Program, Operator).
Sts_Ovrd
BOOL
1 = Override is selected (supersedes External, Program, Operator).
Sts_Ext
BOOL
1 = External is selected (supersedes Program, Operator).
Sts_Prog
BOOL
1 = Program is selected.
Sts_ProgLocked
BOOL
1 = Program is selected and Locked.
Sts_Oper
BOOL
1 = Operator is selected.
Sts_OperLocked
BOOL
1 = Operator is selected and Locked.
Sts_ProgOperSel
BOOL
Program/Operator selection (latch) state: 1 = Program, 0=Operator.
Sts_ProgOperLock
BOOL
Program/Operator lock (latch) state, 1 = Locked, 0=Unlocked.
Sts_Normal
BOOL
1 = Selection equals the Normal (Program or Operator).
Sts_ExtReqInh
BOOL
1 = External request inhibited, cannot get to External from current state.
Sts_ProgReqInh
BOOL
1 = Program request inhibited, cannot get to Program from current state.
Sts_MAcqRcvd
BOOL
1 = Maintenance Acquire command received this scan.
MRdy_OoS
BOOL
1 = Ready for MCmd_OoS, enable HMI button.
MRdy_IS
BOOL
1 = Ready for MCmd_IS, enable HMI button.
MRdy_Acq
BOOL
1 = Ready for MCmd_Acq, enable HMI button.
MRdy_Rel
BOOL
1 = Ready for MCmd_Rel, enable HMI button.
XRdy_Acq
BOOL
1 = Ready for XCmd_Acq, enable HMI button.
XRdy_Rel
BOOL
1 = Ready for XCmd_Rel, enable HMI button.
ORdy_Oper
BOOL
1 = Ready for OCmd_Oper, enable HMI button.
ORdy_Prog
BOOL
1 = Ready for OCmd_Prog, enable HMI button.
ORdy_Lock
BOOL
1 = Ready for OCmd_Lock, enable HMI button.
ORdy_Unlock
BOOL
1 = Ready for OCmd_Unlock, enable HMI button.
ORdy_Normal
BOOL
1 = Ready for OCmd_Normal, enable HMI button.
Out_OwnerSts
DINT
Status of command source, owner command handshake and ready status:
0 = None,
.10 = Operator Lock,
.11 = Operator Unlock,
.12 = Program Lock,
.13 = Program Unlock,
.14 = Acquire Maintenance,
.15 = Release Maintenance,
.16 = Acquire External,
.17 = Release External,
.18 = Has Maintenance,
.19 = External Override Lock,
.20 = Has External,
.21 = Has Operator,
.22 = Has Operator Locked,
.23 = Has Program,
.24 = Has Program Locked,
.29 = Echo,
.30 = Not Ready
Operation
The instruction uses these command sources. The command sources are prioritized in order from highest to lowest in this table.
Command Source
Description
Hand
Hardwired logic or other logic outside the instruction controls the device. The instruction tracks the state of the device for bumpless transfer back to one of the other command sources.
(Highest priority command source)
Out-of-Service
The instruction is disabled and has no owner.
Maintenance
Maintenance controls the device and supersedes Operator, Program, External and Override control. Operator commands and settings from the HMI are accepted.
Override
Priority logic controls the device and supersedes Operator, Program and External control. Override Input (Inp_Ovrd) is accepted.
External
External logic (e.g. field pilot control or upstream SCADA) controls the device. External commands (XCmd_) are accepted.
Program locked
Program logic controls the device. Program commands (PCmd_) are accepted. Operator cannot take control from the Program. Override cannot take control from the Program unless Cfg_OvrdOverLock = 1.
Program
Program logic controls the device. Program commands (PCmd_) are accepted.
Operator locked
The Operator controls the device. Operator commands (OCmd_) from the HMI are accepted. Program cannot take control from Operator. Override cannot take control from Operator unless Cfg_OvrdOverLock = 1.
Operator
The Operator controls the device. Operator commands (OCmd_) from the HMI are accepted.
(Lowest priority command source)
The instruction enables or disablesthese operations:
  • Maintenance Out-of-Service exists
  • Maintenance exists
  • External exists
  • Program (unlocked) exists
  • Program locked exists
  • Operator (unlocked) exists
  • Operator locked exists
  • PCmd_Lock used as a Level (1 = Lock, 0 = Unlock)
The instruction checks for invalid configurations of control and forces the nearest valid configuration.
The core control model arbitrates the source of the commands and parameters that the receiving function accepts. The core control model determines if the source is:
  • A programmatic entity which resides entirely within the processing environment, or
  • An external interface entity which issues commands and parameters external and asynchronously to the processing environment.
Locking a command source prevents the other command source from acquiring privilege.
Core command source model
The core control model consists of these command sources:
  • Oper
  • OperLocked
  • Prog
  • ProgLocked
The control model defaults to this configuration. Other command sources may be present in the model but act as overriding command sources, acting independent of the base Operator/Program state machine.
Enabling command sources as configuration
The individual command sources may be enabled or disabled by the user. The default configuration uses the entire base model; upon power-up of the processing environment the command source will be the designated default. Some combinations of enabled command sources are disallowed as they are either unnecessary or could create unintended changes.
Prog Power Up
Configuration allows the user to specify whether Operator or Program is the power-up default.
Prog Priority
Configuration allows the user to specify whether Operator or Program commands take priority when simultaneously asserted.
Automatic reset of commands
All commands are treated as one-shot-latched. This means that all commands are automatically cleared when the instruction executes and processes them.
Changing Destination States
Under certain configurations the destination command source for some commands may change. This is in keeping with the intent of the command. For example, if the Prog is disabled, the destination of the OCmd_Prog command is directed to the ProgLocked state instead of the Prog state. This maintains the intent of the OCmd_Prog command: the operator entity wishes to place the function in control of the program. If the command was eliminated there would be no way to accomplish this. This is only done in configurations where it would cause no conflict or race condition, but serves to preserve as much user functionality as is practical.
Higher Priority Command Sources
These Higher priority command sources operate independently within the model:
  • External
  • Override
  • Maintenance
  • Out-of-Service
  • In-Service
  • Hand
Initialization
The instruction is normally initialized in the instruction first run. Re-initialization can be requested any time by setting Inp_InitializeReq = 1. For proper initialization, when adding the instruction while performing an online edit of the code, make sure that Inp_InitializeReq = 1 (default value).
Monitor the PCMDSRC Instruction
Use the operator faceplate from the PlantPAx library of Process objects for monitoring.
Affects Math Status Flags
No.
Major/Minor Faults
None specific to this instruction. See Index Through Arrays for array-indexing faults.
Execution
Ladder Diagram
Condition/State
Action Taken
Prescan
Rung-condition-out clears to false.
Sts_eSrc is set to 0. Sts_bSrc is set to 0.
Instruction first run
All commands that are automatically cleared on each execution are cleared and ignored.
The Program/Operator selection is set based on the configuration (Cfg_ProgPwrUp).
The Program or Operator lock selection is set to unlocked.
The Maintenance acquired/released state is not modified and persists through a controller powerup or PROG-to-RUN transition.
Rung-condition-in is false
The instruction is put Out of Service if Inp_Hand=0. The output is de-energized.
Command source selection processing proceeds except that Program and Operators commands are ignored and cleared and all ownership status bits (Sts_Maint, Sts_Ovrd, Sts_Ext, Sts_Prog and Sts_Oper) are cleared to 0. When rung-condition-in becomes true, the Program/Operator selection is set based on the configuration (Cfg_ProgPwrUp).
Rung-condition-in is true
Set rung-condition-out to rung-condition-in.
The instruction executes.
Postscan
Rung-condition-out is cleared to false.
Function Block Diagram
Condition/State
Action Taken
Prescan
EnableOut is cleared to false.
Sts_eSrc is set to 0. Sts_bSrc is set to 0.
Instruction first run
All commands that are automatically cleared on each execution are cleared and ignored.
The Program/Operator selection is set based on the configuration (Cfg_ProgPwrUp).
The Program or Operator lock selection is set to unlocked.
The Maintenance acquired/released state is not modified and persists through a controller powerup or PROG-to-RUN transition.
Instruction first scan
See Instruction first run in the Function Block Diagram table.
EnableIn is false
EnableOut is cleared to false.
The instruction is put Out of Service if Inp_Hand=0. The output is de-energized.
Command source selection processing proceeds except that Program and Operators commands are ignored and cleared and all ownership status bits (Sts_Maint, Sts_Ovrd, Sts_Ext, Sts_Prog and Sts_Oper) are cleared to 0. When rung-condition-in becomes true, the Program/Operator selection is set based on the configuration (Cfg_ProgPwrUp).
EnableIn is true
EnableOut is set to true.
The instruction executes.
Postscan
EnableIn and EnableOut bits are cleared to false.
Structured Text
In Structured Text, EnableIn is always true during normal scan. Therefore, if the instruction is in the control path activated by the logic it will execute.
Condition/State
Action Taken
Prescan
See Prescan in the Ladder Diagram table.
Instruction first run
See Instruction first run in the Ladder Diagram table.
EnableIn is true
See Rung-condition-in is true in the Ladder Diagram table.
Postscan
EnableIn and EnableOut bits are cleared to false.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.