- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Configure CC Function Block tuner
Follow these steps to configure the tuner.
To configure the CC Function Block tuner
- Put all three CV parameters into Manual mode.
- Set the AtuneStart parameter. The tuner starts collecting PV and CV data for noise calculation.
- After collecting 60 samples (60*DeltaT) period, the tuner adds StepSize to the CV.
- Set the AtuneUseModel parameter to copy the tuned parameters to the model parameters. The function block then resets the AtuneUseModel parameter.TIP:
- After successfully collecting the PV data as a result of the CV step change, the CV assumes its value before the step change and the AtuneStatus, GainTuned, TCTuned, DTTuned, and RespTCTuned parameters are updated.
- After a successful AutoTuneDone, the Atune parameter is set to one (1). Tuning completed successfully.
- To identify models and to calculate response time constants for all three CV-PV processes, run the tuner up to three times to obtain CV1-PV, CV2-PV, and CV3-PV models and tuning, respectively.
Provide Feedback