Text box

Text box

Add notes to an SFC or to a Function Block Diagram to clarify a part of the routine, or to capture information that you will use later on.
TIP: If you want the text box to move with the step, instruction, or transition to which it applies, click the pin symbol in the text box and then click the element to which you want to attach it. A green dot shows a valid connection point.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal