Low signal too high

Low signal too high

The Low Signal Scaling value is not less than the High Signal Scaling Value. The Scaling values are entered in module signal units. You must set these output points within the module default signal range. These values are scaled to Engineering values.
Enter a Low Signal that is less than the High Signal.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal