Choose Firmware Revision dialog box settings
Use the
Choose Firmware Revision
dialog box to update the firmware and select the firmware revision for a controller or motion module.
TIP:
If utilizing the
FactoryTalk Linx
edition and using an older version of ControlFlash, the path may be invalid. Change the communication software edition to RSLinx Classic
.These are the settings in the
Choose Firmware Revision
dialog box: Setting | Description |
Module Name | Displays the name of the target module. This item displays:
|
Type | Displays the type of the target module. |
Serial Number | Displays the serial number of the target module. |
Revision | Displays the current firmware revision of the target module. |
Comm Path | Displays the current communications path used to communicate with the target module. |
Look for Firmware Update Files In | The directory containing the available updates. Select a recent selections from the list, or an click the Browse button to navigate to the appropriate directory. |
Browse | Used to navigate to the directory that stores the firmware updates. |
Revision | Displays the revision number of the corresponding firmware update. Note that only those updates which are compatible with the connected module are listed in this table. This list is sorted in descending order, according to revision number, such as the latest firmware revision appears at the top of the list. |
Update Type | Displays Upgrade or Downgrade to indicate the type of revision for the selected file, relative to the current module’s firmware revision. |
File | Displays the path and file name of the .nvs file for the firmware update. The path is relative to the path selected for Look for Firmware Update Files In . |
Installed Firmware Update Files Directory | Displays the root of the update directory for the installed firmware update files on the local workstation. |
Update | Used to start the flash update. |
Provide Feedback