Who Active dialog box
The
Who Active
dialog box contains a communication software edition network interface used to navigate network topologies and configure the access methods used to communicate with devices. Use the
Who Active
dialog box to perform the following tasks:
TIP:
Top open the Who Active dialog:
- SelectCommunications > Who Active.
- Navigate network topologies
- Select, modify, or clear the path thatLogix Designeruses when aGo Online,Upload, orDownloadcommand is initiated.
- Download a project fromLogix Designerto a controller
- Upload a project from a controller toLogix Designer
- Update firmware to a controller
Provide Feedback