Add-On Instruction Definition Editor Dialog - Change History Tab Overview

Use this tab to display attributes regarding when the Add-On Instruction was created and the last time this Add-On Instruction was edited.
Attributes
Created
Displays the date and time when the Add-On Instruction was originally created. Also, identifies who created the instruction.
If the Add-On Instruction is fully-locked, identity information does not display (including the labels), although the Date and Time information is shown.
Edited
Displays the date and time of the last edit to the Add-On Instruction, along with the editor’s identification.
If the Add-On Instruction is fully-locked, this editor information does not display (including the label), although the Date and Time information is shown.
Clear Identities
Click to clear the created by and edited by identity attributes in the Add-On Instruction. The Clear Identities button is hidden if the Add-On Instruction is source-protected.
Logic
Click to open the Logic routine. This Logic button is not visible if the Add-On Instruction is source-protected.
Data Type Size
Displays the size of the Add-On Instruction data type – this does include the size of any Local Tags (even though Local Tags are not visible when an instance tag of this data type is expanded in the Tag Editor or Data Monitor), but it does not include logic size. The size is automatically updated when you apply the instruction, not as you create the Parameters and Local Tags.
Copy all default values of parameters and local tags whose values were modified to all tags of this instruction type
Copies all the default values of the parameters/local tags, or members' default values, that you have changed, to all instance tags of this instruction type.
OK
Click this button to close the Add-On Instruction Definition Editor dialog box.
Cancel
Click this button to close the Add-On Instruction Definition Editor dialog box.
Help
Click this button for help on this tab.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.