- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Add-On Instruction Definition Editor dialog box - General tab
Use the
General
tab on the Add-On Instruction Definition Editor
dialog box to configure the general properties of an Add-On Instruction.
TIP:
To open the Add-On Instruction Definition Editor dialog box - General tab:
- In theController Organizer, expand theAssetsfolder, right-click an Add-On Instruction, and selectProperties.
Provide Feedback