Load Feedback page
The
Load Feedback
page contains information from the feedback device that is directly coupled to the load-side of a mechanical transmission or actuator. Use the Load Feedback
page to enter load feedback-device information.The
Load Feedback
page is available when Feedback Configuration
on the General
page is set to Load
or Dual Feedback
.
TIP:
The controls on this tab are available when the controller is offline.
TIP:
To open the Load Feedback page:
- In theController Organizer, expand theMotion Groupsfolder, and double-click an axis.
- From theAxis Propertiesdialog box, inCategories, selectLoadFeedback.
Parameter | Description |
---|---|
Device Function | Displays the feedback device function as Load-Side Feedback. |
Feedback Channel | Displays the CIP motion feedback channel as Channel 2. |
Type | Selects the type of feedback device. Each feedback device has different configuration parameters. The following is a list of available types: Integrated SSI Sine/Cosine SSI AqB BiSS Sine/Cosine Not Specified Digital AqB Digital AqB (With UVW) Digital Parallel (Abs) Sine Cosine Sine Cosine (With UVW) Hiperface EnDat Sine/Cosine EnDat Digital Resolver SSI Digital LDT Hyperface DSL BiSS Digital Tamagawa Serial Stahl SSI Not Specified is the default parameter. |
Units | Select the required unit. The available units are:
|
Parameters | Opens the Motion Axis Parameters page to modify existing or additional parameters.Tip: The Parameter List page may contain more attributes than the associated page. In some cases, attributes that display on the Parameter List page do not display on the associated page. |
Device Type parameters | The device Type parameters display when device Type is set to any value, except Not Specified .Tip: The device type determines which parameters appear on the page. Parameters not supported by the device type are hidden. |
Cycle Resolution | Enter the cycle resolution for the feedback device. |
Cycle Interpolation | Enter the interpolation factor for the feedback device. Valid values include:
|
Effective Resolution | Displays the effective resolution of the feedback device. This value is calculated by multiplying the Cycle Resolution with the Interpolation Factor . |
Startup Method | Select the startup method for the feedback device. This parameter determines how the device applies the feedback count value during drive startup. Valid values include:
|
Commutation Offset | Enter a value for the commutation offset. Tip: This value and the Commutation button only display for feedback devices that support commutation offset. |
Test Commutation | Opens a dialog box to perform a commutation test (Hookup Test) on the device. |
Data Code Type | Select a data type code for the feedback device. The available options are:
|
Data Length | Enter the length of the data in bits. |
Absolute Turns/Absolute Length | For a rotary motor, enter the absolute number of turns for the device to make. For a linear motor, enter the absolute length of the device. |
Transformation Ratio | Enter the transformation ratio of the feedback device. |
Feedback Ratio | Enter the feedback ratio between the Load Feedback and the Motor Mounted Feedback. |
Provide Feedback