Guidelines to drag and drop cursors

Guidelines to drag and drop cursors

You can drag-and-drop items from the
Controller Organizer
to a different project in a different copy of the
Logix Designer
application. You can quickly build new projects by copying from a library project or from a similar project. You can drag-and-drop an item from the
Controller Organizer
to the
Controller Organizer
or the
Logical Organizer
in the different project.
When you drop the item on a target in the different project, a copy of the dropped item appears under the target. If a dragged program has any descendant programs (defined in the
Logical Organizer
), they are not copied when using drag-and-drop from the
Controller Organizer
.
Description
Cursor
Move cursor that appears where you can drop the item (click and drag)
RSL5K_MoveCursor_v31
Copy cursor that appears where you can drop a copy of the item (
Ctrl
+click and drag)
RSL5K_CopyCursor_v31
NOT cursor that appears where you cannot drop an item.
RSL5K_NoNoCursor_v31
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal