- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Change the Safety Network Number (SNN)
The CIP Safety protocol is an end-node to end-node safety protocol that allows routing of CIP Safety messages to and from CIP Safety devices through bridges, switches, and routers. To prevent errors in non-certified bridges, switches, or routers from becoming dangerous, each end node port that is within a routable CIP Safety control system must have a unique node reference. This unique reference is a combination of a Safety Network Number (SNN) and the node address.
A time-based Safety Network Number is automatically assigned by the software when the safety project is created or when changing the IP Mode for
CompactLogix
5380 controllers. The time-based format is based on the creation date and time (to the millisecond). The Safety Network Number can also be entered manually.Use the
Safety
tab on the Controller Properties
dialog box to view or change the Safety Network Number. The Safety
tab displays the safety network number for each port that supports a CIP Safety connection. Some controllers, such as the GuardLogix
5580 and CompactLogix
5380, may have multiple Safety ports.Before you begin:
- Unlock the project if it is safety-locked.
- Delete the safety signature if a safety signature exists.
To change the SNN:
- On theOnlinetoolbar, select theController Propertiesicon.
- In theController Propertiesdialog box, select theSafetytab.
- Select
to the right of the
Safety Network Numberto change. TheSafety Network Numberdialog box opens. - Do one of these actions:
- SelectTime-basedand then selectGenerateto have the software assign the SNN.
- SelectManualand then enter a number between 1 and 9999.The Safety Network Number appears in theNumberbox.
- SelectOK.
Provide Feedback