Controller Properties dialog box - Major Faults tab
Use the
Major Faults
tab on the Controller Properties
dialog box to display information on the major faults that occurred in the controller.
TIP:
To open the Controller Properties dialog box - Major Faults tab:
- On theOnlinetoolbar, click theController Propertiesicon.
- On theController Propertiesdialog box, click theMajor Faultstab.
TIP:
This tab can also appear on the
Connected
dialog box to view and clear major faults without having to first correlate with the controller. Provide Feedback