Add a sequence element using the Equipment Sequence Element toolbar

Add disconnected sequence elements to the
Equipment Sequence
diagram. Note that when selecting a transition, and adding a Step and Transition pair, it is automatically inserted below the selected transition.
  1. Click the Sequence Editor workspace.
  2. On the
    Equipment Sequence
    Element
    toolbar, click the button for the element to add.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.