Add a step and transition pair
Use
to add a step and transition pair. Although added as a pair, you can select and edit each element separately.
Add Step and Transition Pair

To add a step and transition pair:
- Select in the Sequence Editor workspace, or select on an element to connect to in the sequence diagram.
- On theEquipment SequenceElement toolbar, selectAdd Step and Transition Pair
.
- Select the connector of the first element to create a link, and then select the connector of the second element to attach the link.TIP:If you select a transition before adding a Step and Transition Pair, the Step and Transition Pair automatically inserts below the selected transition.
Provide Feedback