Configure the step name after adding to an Equipment Sequence
After adding a disconnected step or a step and transition pair to an
Equipment Sequence
diagram, configure the step name.To configure the step name after adding to an
Equipment Sequence
:- Find and select the step in theEquipment Sequence.
- Double-click the default step name text and rename the step to reflect the process.TIP:Changing the name of the step automatically changes the name of all step tags and updates references to those step tags (like transition expressions and parameter expressions).The transition expression referencing a step attribute automatically updates the step name in the transition. For example, fromOldStepName.CompletetoNewStepName.Complete.
Provide Feedback