Resolve import conflicts when importing an Equipment Sequence

Resolve import conflicts when importing an Equipment Sequence

When you import an Equipment Sequence, the settings and references in the imported Equipment Sequence sometimes conflict with settings that exist in your project. You use the Import Configuration dialog box to view and resolve conflicts.
The following table describes the icons in the Import Content pane that indicate when differences or conflicts exist between imported and existing settings.
Icon
Description
Import_Configuration_dialog_warning_flag_without_astericks
Indicates a potential import problem.
general_differences_icon (2)
Indicates that differences exist between the imported Equipment Sequence and the existing project. The differences are not necessarily conflicts, however.
Import_Configuration_dialog_warning_flag
Indicates that new errors or messages have been added to the
Import Content
pane or that previous errors or messages have been removed since the last time you accessed the pane.
To view and resolve import conflicts:
  1. In the
    Import Content
    pane, click the item that has a difference or error indicator next to it. A settings table for that item appears in the Details pane.
  2. Adjust the settings in the table to resolve the conflicts.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal