Failed to set Dialog Field Name value

Failed to set Dialog Field Name value

You selected
OK
or
Apply
on the configuration dialog box, but the value in the field in the dialog box is invalid. This could occur because:
  • The tag was deleted.
  • There is an invalid numeric value for the type of field (that is, if the field is expecting an integer, and you enter a real value).
  • Insufficient memory.
  • You specified an element or member of a tag as the (local) Source or Destination for a message
You must specify a complete tag. Additionally, if you want to start a message in the middle of a local structured tag, you can create an alias tag to the location of where you want to start.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.