- Studio 5000 Logix Designer
- Tasks, programs, and routines
- Add-On Instructions
- Controller Organizer
- Logical Organizer
- Alarms
- Tag-based alarms
- Tag Editor and Data Monitor
- Configure settings for Tag Editor and Data Monitor
- Equipment phases
- Equipment Sequences
- Equipment Sequence Diagrams
- Ladder Editor
- Structured Text Editor
- Sequential Function Chart Editor
- Define the steps of an SFC process
- PlantPAx instruction properties
- Controller Properties
- Editing Controller Properties
- Controller Security
- Source Protection
- License Source Protection for Routines and Add-On Instructions
- Module Information
- 1756 ControlLogix I/O Modules
- Instruction Set
Function Block Properties dialog box - Configure tab (D2SD)
The Discrete 2-State Device (D2SD) instruction controls a discrete device which has only two possible states (e.g., on/off, open/closed, etc).
Use the
Configure
tab to set the parameter values for the selected (D2SD) function block.The following table describes the parameters available on the
Configure
tab:Parameter | Description |
Feedback States | Click one or more of the four buttons to configure the state of the feedback (FB0 or FB1) when the device is in a 0 or 1 state. The options are:
|
Output Reverse | Select this check box to reverse the default output state. |
Fault | |
| Enter the value (in seconds) of the time to allow the device to reach a newly commanded state. Setting a Fault Time of zero disables the fault timer. If you enter an invalid value, the instruction will assume a value of zero and set a unique bit in Status. |
| Select this check box to latch the fault alarm. |
Override | |
| Used to configure the state of the device when the device is in Override mode. A value of 0 indicates that the device should go to the FALSE, or 0, state. A value of 1 indicates that the device should go to the TRUE, or 1, state. |
| Select this check box to set the 2-State Device to Operator control. If this box is not selected, the 2-State Device will execute normally. |
| Select this check box if you want the device to go to Override mode and enter an Override state on a fault alarm. After the fault alarm is removed, the device will be placed in Operator mode. |
Program value reset | Select this check box to reset the program control values. |
Status | Displays read-only status information for blocks containing status bits. If none of the status bits are set, an OK message appears in this field. Otherwise, a list of the status bits that are set appears here. This list is comprised of the parameter names associated with the status bits, and typically explain which parameters were configured with invalid values. |
Execution Order Number | Displays the block's execution number if the routine is in a verified state. If the routine is not yet verified, a Routine not verified message displays. Note that this item is read-only. |
Never display description in a routine | Select this check box if you do not want the description to display in the routine. |
OK | Click this button to add the selected item in the instruction list to the routine and close the Fun ction Block Properties dialog box. |
Cancel | Click this button to cancel any edits you have made and close the Function Block Properties dialog box. |
Apply | Click this button to accept your changes and continue editing in the Function Block Properties dialog box. |
Provide Feedback