Copy and paste components using Paste Special commands

Copy and paste components using Paste Special commands

Use the
Paste Special
commands to copy and paste project components in the
Logical Organizer
and the
Controller Organizer
. The
Paste Special
commands are available when copying from the Controller Organizer to the Logical Organizer, or vice versa.
Paste Special With Configuration
pastes a component and its full configuration.
Paste Special Without Connections
pastes a component without any internal connections (a connection within a program or program's descendants) or external connections (connections outside a hierarchy).
TIP:
If FactoryTalk Security is enabled, you need FactoryTalk security permissions to create and delete items in the
Controller Organizer
and the
Logical Organizer
.
To copy and paste using Paste Special commands:
  1. In the
    Controller Organizer
    or the
    Logical Organizer
    , right-click the item that you want to copy and select
    Copy
    .
  2. Right-click the target item in the Organizer, and select a
    Paste Special
    command:
    • Paste Special > With Configuration
      . In the
      Paste Configuration
      dialog box, rename and configure the item before pasting it.
      Use this command to configure and rename a program, Add-On Instruction, User-Defined Data Type, or string before pasting it in the Controller Organizer or the Logical Organizer. You can also use
      Paste Special with Configuration
      when pasting a folder in the Logical Organizer.
    • Paste Special > Without Connections
      . The copied item is pasted into the Organizer without its connections.
      Use this command to paste a program without its parameter connections in the
      Controller Organizer
      or the
      Logical Organizer
      . You can also use
      Paste Special Without Connections
      when pasting a folder in the
      Logical Organizer
      . This is useful when you want to duplicate programs without any internal connections (a connection within a program or program's descendants) or external connections (connections outside a hierarchy).
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal