PBL output gate
Use the
Advanced - Output gate
tab of the PBL Properties
dialog box to select the source for the output of a PBL instruction. Configure the output gate for a Process Boolean Logic (PBL) instruction
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Under theAdvancedtab, selectOutput gate.
- On theSelect sourcemenu, select the source for the output.
- Select theInvertcheckbox to invert, or reverse, the output value.
- Configure delay timers for outputs:
- Off delay time. Enter an Off delay time in seconds. A delay helps prevent false trips of the output.
- On delay time. Enter an On delay time in seconds. A delay helps prevent spurious trips of the output.
- When online with the controller, monitor theDevice stateandDevice issuesindicators at the bottom left of the dialog box:
- Device state. Displays the current device state depending on the value of the Out_Live parameter. Use theHMItab to enter text in theText to display when output equals 0andText to display when output equals 1boxes.
- Device issues. Displays fault conditions:None, orConfiguration error.
- SelectApply.
Provide Feedback