Alarm conditions for PDBC
Use the
Alarms
tab on the PDBC Properties
dialog box to set the values that define alarm conditions for the instruction.Define alarm conditions for Process Deadband Controller (PDBC) instructions
- On the instruction in the routine, perform one of these actions:
- On the Ladder or FBD instruction, select
.
- In the Structured Text editor, right-click the tag name and selectConfigure <tag name>.
- Select theAlarmstab.
- Configure these settings:
- Use Alarm. Select to use an alarm. Alarm conditions are not evaluated when an alarm is not in use.
- Alarm Name. Enter the label to display for the associated alarm.
- Gate delay. The alarm condition detection is enabled or gated by the gate signal. Gate signals are inputs of the PDBC instruction. Enter a delay in seconds to set the delay for High deviation, Low deviation, High rate of change increasing, and High rate of change decreasing detection.
- Limit. The PV deviation threshold or rate of change threshold for triggering the alarm.
- Deadband. Sets the deadband around the limit. The deadband defines a range above or below the limit to prevent unwanted rapid switching of the status.
- State. The state of the alarm. Hover over the state icon to see a tool tip that describes the alarm state or fault status.An alarm can be in more than one state at a time. For example, an alarm can be in alarm, acknowledged, and suppressed; or normal, unacknowledged, and suppressed.Alarm state icons include:
- Normal, acknowledged (no icon).
- Normal, unacknowledged -
- In alarm, acknowledged -
- In alarm, unacknowledged -
- Suppressed -
- Shelved -
- Disabled -
- Alarm fault -
- To open theAlarm Propertiesdialog box for the alarm, select theConfigurationicon
.
- To configure settings for all pre-defined alarms for a PDBC instruction, selectSettings for all alarms. When this box is checked, changes made to these settings are applied to all pre-defined alarms:
- Class. A group name for related alarms. The class does not limit the alarms that an Alarm Summary object subscribes to. UseClassto filter the alarms that are displayed to the operator.
- Alarm group. A group name to help classify and sort alarms.
- . AFactoryTalk ViewcommandFactoryTalk Viewcommand that can be run on the operator station when the alarm notification appears. Enter the exact syntax for theFactoryTalk Viewcommand.
- To allow an operator to shelve an alarm, selectAllow operator to shelve alarm.
- To allow maintenance technicians to disable an alarm, selectAllow maintenance to disable alarm.
- When online with the controller, monitor theDevice state,Device issues, andDevice modeindicators at the bottom left of the dialog box:
- Device state. When theLogix Designerapplication is online with the controller, displays the current device state:
- Deadband, Q is off
- Deadband, Q is on
- Above Lower setpoint
- Below Raise setpoint
- Same in manual
- Out of service
- Device issues. When theLogix Designerapplication is online with the controller, displays fault status:
- None
- Low deviation
- High deviation
- High rate of change (decreasing)
- High rate of change (increasing)
- Input source bad
- Configuration error
- Device mode. When theLogix Designerapplication is online with the controller, displays the current device mode:
- Auto
- Manual
- Normal
- SelectApply.
Provide Feedback