Transition Properties - General

Use
Transition Properties - General
to specify whether or not to transition descriptions display within the routine view.
Parameter
Description
Never display description in routine
Select to hide the transition’s description within the sequential function chart routine. The description is hidden even if Workstation Options dialog is set to show descriptions.
This check box applies to the current transition only; if the Workstation Options dialog is set to show descriptions, other transition descriptions may be shown unless individually hidden.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.