Documentation Languages toolbar

Use the Documentation Languages toolbar to associate the project's documentation with a language.
doc_languages_toolbar_v31
Use the Documentation Languages toolbar to switch the currently used documentation language. Change the selection in the
Current Language
box to dynamically change the language used to display all project documentation. This toolbar is the quickest, most convenient way to switch a language dynamically in the project.
Use this toolbar to select languages that do not currently have content. If no default language is chosen, the result is blank project documentation for the project.
doc_languages_contentIcon_v31
Languages with content are marked with this icon, indicating that the language has documentation associated with it.
doc_languages_button_v31
The
Documentation Languages
button opens the
Project Documentation Language Configuration
dialog box.
Unless a current language has been specified,
Select a Language
appears in the
Current Language
box. Otherwise, the last language used in the project appears.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.