Run a trend

Run a trend

To be able to run the current trend the workstation must be online to the controller, with the chart open, and have at least one tag configured.
When a trend is started, all existing trend data is permanently deleted.
To run a trend:
  • Select the
    Run
    button on the
    Trend Control
    bar.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal