Trend Control Bar Overview
The trend control bar is used to start and stop trend data sampling. This control bar also displays the current state of the trend in the controller, data collection mode, and sampling type information.
Buttons/Parameters
Button | Usage |
Run | Select this button to start data sampling in the controller. This button is disabled when offline, or when a trend is running. |
Stop | Select this button to stop data sampling in the controller. This button is disabled when offline, or when a trend is stopped. |
Error | Select this button to see trend errors that have been logged against the selected trend. This button is disabled if there are no errors logged against the selected trend. |
Log | Select this button to save the trend log. This button is disabled if there is no trend data in the Trend Chart window. |
Capture | Select the up or down arrow, or enter a value to view a specific capture. This item is disabled if the trend contains only a single capture. |
Provide Feedback