use_factorytalk_security_with_the_logix_designer_application

Use FactoryTalk Security with the Logix Designer application

About the Security Feature

The Security feature lets you control the individual users’ access to the Logix Designer application projects and controllers. Using FactoryTalk Security software, you control access to your projects and controllers based on the following:
  • The individual user logged into a workstation
  • The project the user is attempting to access
  • The workstation from which the user is attempting to access the project
For details see the FactoryTalk Security System Configuration Guide:
Start > Programs > Rockwell Software > FactoryTalk Tools > FactoryTalk Security System Configuration Guide
.
NOTE: The security feature is primarily intended to prevent accidental unauthorized access to your projects and controllers. It is important to note that while the feature does provide some protection against intentional unauthorized access, it is not intended to provide protection against sophisticated system hackers. You should exercise your own additional precautions against such unwanted access.
FactoryTalk Security grants or denies access based on the following pieces of information.
  • User ID (that is, the user’s login name)
  • Workstation ID
  • Action name (that is, the activity the user is trying to perform, such as tag modification, or processor mode change)
  • Resource name (that is, controller name)
In addition, you can group resources, actions, persons, and workstations via access control lists, which define certain characteristics to determine access levels.

Launching the Logix Designer application from a remote computer

To allow users to launch the application from a remote computer may require changing the default security settings in the FactoryTalk Network Directory.
When logging on remotely and trying to launch the application, the user is prompted to Log On to FactoryTalk. After providing the proper credentials, the user is still unable to log on. This happens because the policy Require computer accounts for all client machines is enabled by default and the remote computer is not in the FactoryTalk Directory computer list.
To resolve the remote access issue:
  • Add the remote computer to the FactoryTalk Network Directory or
  • Change the security policy setting, Identify terminal server clients using the name of to Server Computer.
For details see Set up security policies and Add a computer account in the
FactoryTalk Administration Console
help.
NOTE: In the case where a FactoryTalk administrator is logged on to the FactoryTalk Network Directory and Single Single-on is enabled, the client launches the Logix Designer application using the active administrator account. For details see Single Sign-on in the
FactoryTalk Administration Console
help.

The Logix Designer application and FactoryTalk security

When used with the Logix Designer application, FactoryTalk Security supports Product Policies and Securable Actions. These FactoryTalk Security settings are configured in the FactoryTalk Administration Console.
Product Policies are not tied to a specific project, and may include the following.
  • Securing the controller
  • Creating a new project (either through the New Controller dialog box, or through the Translator Tool utility)
  • Updating your firmware
Securable Actions let you perform specific tasks on a specific project or group of projects, and may include the following.
  • Viewing a project
  • Going online
  • Creating tags
  • Creating modules
In a safety controller project, you can specify additional protection to safety components. For example, to create a safety program, you need to have access granted for both of these securable actions:
  • Safety: Modify Component
  • Program: Create
In the
Logix Designer
application:
  • Security settings are obtained from the FactoryTalk Network Directory.
  • RSSecurity Emulator is not used by the Logix Designer application, but may be required by other software.
  • FactoryTalk Local directory is not supported.
  • FactoryTalk Services Platform version 2.50 (SR5) or later supports associating the project with a specific FactoryTalk Directory.

Product policies and securable actions

The Product Policies and Securable Actions listed here are configured in the Network Directory using the FactoryTalk Administration Console. For details see the
FactoryTalk Security System Configuration Guide
.

Product policies

Grant access to these actions
To allow a user to
Controller: Secure
Secure a project or controller.
Firmware: Update
Update controller firmware.
NOTE: If the project is secured, the Securable Action (Firmware:Update) is also required to perform firmware updates. Firmware updates can be initiated within the Logix Designer application WhoActive dialog box if a project is open but not when the controller is online.
Print: Modify Options
Modify print options.
Project: New
Create a new project, import a project or translate PLC5/SLC.
Toolbar: Configure
Move, resize, hide or show toolbars.
Workstation: Modify Options
Modify workstation options.

Securable actions

Grant access to these actions
To allow a user to
Add-On Instruction: Create
Create a new Add-On Instruction.
Add-On Instruction: Delete
Delete an Add-On Instruction.
Add-On Instruction: Modify
Edit Add-On Instruction properties, tags, logic or whether a user can configure source protection.
Alarm: Clear Alarm Log
Clear the contents of the alarm log from the controller.
Controller: Clear Faults
Edit the fault log, including clearing faults.
Controller: Lock/Unlock
Lock or unlock the controller for online edits.
Controller: Modify Mode
Change controller modes.
Controller: Modify Properties
Edit controller properties.
Controller: Modify Revision
Convert the .acd file to a higher revision.
Controller: Modify Type
Change controller types.
Note:
If a user is granted Controller: Modify Revision privilege, but is denied Controller: Modify Type, then he will typically be unable to change the type of controller. However, during database conversion, it may be necessary to change the controller type because the old controller type is obsolete in the target revision. In this case, these users are allowed to change the controller type during conversion.
Controller: Unsecure
Unsecure a secured controller.
Firmware: Update
Use the Logix Designer application to update controller firmware.
Note:
The Product Policy (Firmware:Update) is also required to perform firmware updates. Firmware updates can be initiated within the Logix Designer application WhoActive dialog box if a project is open, but not when the controller is online.
Language: Modify Properties
Associate project documentation with a language, set default language, add or delete a language.
Language: Switch Language
Select a different language for product documentation.
Module: Create
Create modules in the Controller Organizer.
Module: Create and Safety: Modify Component
Create safety I/O configuration.
Module: Delete
Delete modules in the Controller Organizer.
Module: Delete and Safety: Modify Component
Delete safety I/O configuration.
Module: Maintenance High
Perform high impact operations such as module reset and calibration.
Module: Maintenance Low
Perform low impact operations such as resetting electronic fuses.
Module: Modify Properties
Edit module properties.
Module: Modify Properties and Safety: Modify Component
Modify safety I/O configuration.
Motion: Command Axis
Perform axis direct commands.
Motion: Modify Configuration
Modify axis, coordinate system, or motion group properties.
Nonvolatile Memory: Load
Load from non-volatile memory.
Nonvolatile Memory: Store
Store to non-volatile memory.
Phase: Create
Create equipment phases.
Phase: Delete
Delete equipment phases.
Phase: Manual Control
Manually control equipment phases.
Phase: Modify Properties
Edit equipment phases.
PLC/SLC: Modify Tag Mappings
Map PLC or SLC messages.
Print: Report
Print reports.
Program: Create
Create programs.
Program: Create and Safety: Modify Component
Create a safety program.
Program: Delete
Delete programs.
Program: Delete and Safety: Modify Component
Delete a safety program.
Program: Modify Properties
Edit program properties.
Program: Modify Properties and Safety: Modify Component
2
Modify properties of a safety program.
Program: Modify Properties and Safety: Modify Component
Change class property of a standard program to safety.
Project: Compact
Compact a project file.
Project: Download
Download a project to a controller.
Project: Export
Save a project in .L5K or .L5X format.
Project: Go Online
Go online with a project.
Project: Modify Path
Set, clear, or modify the controller path associated with a given project.
Project: Open
Open a (read-only) version of the project.
Note:
If users do not have the ability to open and view the project, they do not have the ability to do anything else with it.
Project: Save
Save a project.
Project: Save As
Save a project to a new .acd file.
Project: Upload
Upload a project from a controller.
Routine: Create
Create a routine.
Routine: Create and Safety: Modify Component
Create a safety routine.
Routine: Delete
Delete a routine.
Routine: Delete and Safety: Modify Component
Delete a safety routine.
Routine: Manual Control
Manually control routine logic.
Routine: Modify Logic
Edit routine logic.
Routine: Modify Logic and Safety: Modify Component
Edit safety routine logic.
Routine: Modify Properties
Edit routine properties, configure routine source protection.
Routine: Modify Properties and Safety: Modify Component
Edit safety routine properties.
Safety: Generate/Delete Signature
Generate or delete a Safety Signature.
Safety: Lock/Unlock
Lock or unlock edits on safety application.
Safety: Lock/Unlock
Modify safety lock or unlock passwords.
Safety: Modify Component
Create, delete, or modify safety components.
Note:
The standard component privileges are required in addition to this privilege. For example, to create safety tags, Tag: Create is required in addition to Safety: Modify Components.
Safety: Modify Properties
Modify the controller's safety configuration.
Safety: Modify Tag Mappings
Create safety tag mapping.
Safety: Modify Tag Mappings
Delete safety tag mapping.
Safety: Modify Tag Mappings
Modify safety tags mapped to standard tags.
Tag: Create
Create tags.
Tag: Create and Safety: Modify Component
Create a safety tag.
Tag: Delete
Delete tags.
Tag: Delete and Safety: Modify Component
Delete a safety tag.
Tag: Delete, Safety: Modify Tag Mappings, and Safety: Modify
Delete standard tag that is mapped to a safety tag.
Tag: Force
Force tags and enable or disable existing forces.
Tag: Force and Safety: Modify Component
Force safety tags.
Tag: Modify Constant Property
Change Constant property of a tag.
Tag: Modify Constant Tag Values
Change values of a Constant Tag.
Tag: Modify Properties
Edit tag properties.
Tag: Modify Properties and Safety: Modify Component
Edit safety tag properties.
Tag: Modify Properties and Safety: Modify Component
Change class property of a standard tag to safety.
Tag: Modify Properties and Safety: Modify Tag Mappings
Modify safety or standard tag properties of a tag contained in a safety mapping.
Tag: Modify Values
Change tag values.
Tag: Modify Values and Safety: Modify Component
Change safety tag values.
Task: Create
Create tasks.
Task: Delete
Delete tasks.
Task: Modify Properties
Edit task properties, including program scheduling.
Task: Modify Properties and Safety: Modify Component
1
Modify safety task properties.
Trend: Create
Create trends.
Trend: Delete
Delete trends.
Trend: Modify Properties
Modify trend properties.
Trend: Run
Run trends.
User Defined Type: Create
Create user-defined data types or string types.
User Defined Type: Delete
Delete user-defined data types or string types.
User Defined Type: Modify
Edit user-defined data types or string types.
Note 1: The safety task max scan time and max/min interval scan timers can be reset, regardless of the protection.
Note 2: A safety program’s max scan time can be reset, regardless of the protection.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.
Normal