As a global leader in providing packaging solutions in the food and pharmaceutical segment, Bosch Packaging, Goa, India supplies horizontal form fill and seal machines primarily to the bakery and confectionery industries. The company plans to gratify the omnipresent and ever-growing demands from the Indian packaging market through Bosch Packaging’s Goa facility with its fully equipped R&D facility, engineering and after-sale support, and sophisticated assembly shop floor to build machines with advanced technology.
The designing of customized projects poses the distinct challenge of containing a common engineering component which can be reutilised in other similar projects. This is a challenge that engineers at in Goa, India are all too familiar with.
Often, for their customized line solutions, Bosch Packaging is required to design a Product Distribution System (PDS) to feed product into down-stream wrapper lines. The time required to engineer these systems is a significant factor impacting project delivery schedules. The biggest challenge is to have a common engineered solution that can be re-used for various similar projects.
The challenges imposed due to the variability of customized project demands include:
- Variation in line speed
- Variation in total number of downstream flow wraps
- Variation in each of flow wrap speed and dynamics of flow wrap
- Protection of IP while automation applied to PDS solution
Bosch Packaging, Goa, India found that while the engineering time spent for each project was huge, maintaining consistency in the application code over various projects was also a challenge, and thereby impacted maintainability.
Another area of concern was the high installation time. This drawback occurred due to the limitation of handling data over higher number of nodes (drives) which existed in the MODBUS communication network.