Add-On Instruction elements
This table describes add-on instruction elements.
Element | Description |
---|---|
Description | Text that describes the add-on instruction. |
Parameters | Parameters of the add-on instruction. |
LocalTags | Local tags for the add-on instruction. |
Routines | Logic that makes up the add-on instruction. |
Provide Feedback