Keyboard Shortcuts
If you prefer navigating the interface with the keyboard, here are some tips to help you move efficiently.
- Select the arrow keys to move up, down, left, and right within the grid.
- SelectCtrl+ the left arrow key to move to select the end of the row.
- SelectCtrl+ the right arrow key to move to the beginning of the row.
- Select thePage upkey to move up an entire screen.
- Select thePage downkey to move down an entire screen.
- Expand groups by moving to the group item and then selecting theEnterkey.
- Edit an item in the grid by moving to the item and then selecting theEnterkey. Some items are read-only.
- Select theSpacebarto select an entire row.
- Move the focus to the column headers to access sorting and filtering. When in the header row:
- Select theSpacebarto toggle the header checkbox to show or hide the column.
- Select theEnterkey to toggle the sorting state of the column.
- SelectCtrl+ theEnterkey to open the menu for that header.
- SelectEscto close the menu.
Provide Feedback