Module Fault Icon
The Module Fault Icon is a yellow exclamation mark (!) with a triangle around it.
The I/O Configuration Folder (top level) displays the Module Fault Icon if a module below it is faulted; it does not display the Module Fault Icon if the module is inhibited, waiting, etc.
Each individual module icon displays the Module Fault Icon if the module is not running; in other words, it appears for all states except for running. For example, it appears if the module is:
- faulted
- waiting
- etc.
Provide Feedback