The Sequence Manager

The Sequence Manager models and executes sequential manufacturing processes using the
ControlLogix
features described in these tasks:
  • Use the
    Equipment Sequence
    Editor to configure the coordination of equipment phase execution.
  • Use ControlLogix to execute equipment sequence programs.
  • Use the
    Logix Designer
    application to monitor and manage running equipment sequences.
  • Add Sequence Manager ActiveX controls to the
    FactoryTalk View SE
    displays to enable operators to monitor and manage running equipment sequences and equipment phases.
  • Use the Sequence Manager Event Client Service and the Sequence Manager Event Archiving Service to subscribe and collect generated sequence events.
Provide Feedback
Have questions or feedback about this documentation? Please submit your feedback here.