Print > Controller Organizer command
The Controller Organizer Listing provides you with a report that lists the basic organization of a project as listed in the Controller. The report is broken up into the following sections:
- Tasks
- Motion Groups,
- Add-On Instructions
- Data Types
- Trends
- I/O Configuration
Components that have descriptions are shown with the descriptions displayed underneath the component. There is no information about tag collections in the report.
Provide Feedback