Project Documentation Language Configuration dialog box overview
Use the Project Documentation Language Configuration dialog box to isolate Project Documentation Languages operations to a location.
These are the parameters for the Project Documentation Language Configuration dialog box:
Parameter | Description |
---|---|
Current | Switch the currently used documentation language, which changes the language used to display all project documentation. You can select languages that do not currently have content. The result is blank project documentation if no default language is selected is displayed for the project. d Select a Language is the default message that is displayed in this field if a current language has not been specified. Otherwise, the last current language used in the project is displayed. |
Default | Select a language to display for project documentation if localization does not exist in the current language. Only the languages that have project documentation content are available for selection. The default is None, unless a current language has been specified. Otherwise, the default is the last language that was used in the project. |
Custom | Opens the Custom Language Configuration dialog box to manage the customized languages in the project. |
Export | Launches the localization of a file. Export appears dimmed if a current language has not been configured. |
Import | Add the contents of a localized file to the project. Import appears dimmed if no current language has been configured. |
Remove | Opens the Remove All Project Documentation dialog box in which you can remove a language localization that is currently in the project. Note that once a language is removed, all localization associated with that language is no longer accessible from the project. Remove appears dimmed if no languages exist in the project. |
Advanced | Opens the Advanced Project Documentation Configuration dialog box to configure the language localization that is downloaded to the controller. The controller is currently the only component in which documentation is stored. Because it is not possible to download all languages to the controller, you must choose one language to download. |
The language with content icon indicates the language has documentation associated with it. The default language is represented by the default language icon .
Provide Feedback